Solid Edge FrameworkSupport Type Library
AttributeSets Property
Description
Returns the AttributeSets collection object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property AttributeSets As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCurves As solidedgeframeworksupport.Curves2d
    Dim objCurve As solidedgeframeworksupport.Curve2d
    Dim dblPoint(1 To 8) As Double
    Dim objCurveAttribSets As Object
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Curves collection
    Set objCurves = objSheet.Curves2d
    'Defining points.
    dblPoint(1) = 0.15
    dblPoint(2) = 0.15
    dblPoint(3) = 0.25
    dblPoint(4) = 0.15
    dblPoint(5) = 0.25
    dblPoint(6) = 0.25
    dblPoint(7) = 0.15
    dblPoint(8) = 0.25
    'Creating a curve on the defined points
    Set objCurve = objCurves.AddByPoints(Pointcount:=4, Points:=dblPoint, FitType:=igDirectFit, Closed:=True)
    'Get Attributesets
    Set objCurveAttribSets = objCurve.AttributeSets





    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCurves = Nothing
    Set objCurve = Nothing
End Sub
See Also

Curve2d Object  | Curve2d Members