Solid Edge FrameworkSupport Type Library
BringToFront Method
Description
Changes the display order of the referenced object by moving it in front of all other overlapping objects.
Syntax
Visual Basic
Public Sub BringToFront() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCurves As solidedgeframeworksupport.Curves2d
    Dim objCurve1 As solidedgeframeworksupport.Curve2d
    Dim objCurve2 As solidedgeframeworksupport.Curve2d
    Dim objCurve3 As solidedgeframeworksupport.Curve2d
    Dim dblPoint(1 To 10) As Double
    Dim lngCurve1Zorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create curves collection
    Set objCurves = objSheet.Curves2d
    'Define points
    dblPoint(1) = 0.15
    dblPoint(2) = 0.15
    dblPoint(3) = 0.25
    dblPoint(4) = 0.15
    dblPoint(5) = 0.25
    dblPoint(6) = 0.25
    dblPoint(7) = 0.15
    dblPoint(8) = 0.25
    dblPoint(9) = 0.1
    dblPoint(10) = 0.1
    'Create curves on the defined points
    Set objCurve1 = objCurves.AddByPoints(Pointcount:=3, Points:=dblPoint, FitType:=igDirectFit, Closed:=True)
    Set objCurve2 = objCurves.AddByPoints(Pointcount:=4, Points:=dblPoint, FitType:=igDirectFit, Closed:=True)
    Set objCurve3 = objCurves.AddByPoints(Pointcount:=5, Points:=dblPoint, FitType:=igDirectFit, Closed:=True)
    lngCurve1Zorder = objCurve1.ZOrder
    'Call BringToFront method.
    Call objCurve1.BringToFront

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCurves = Nothing
    Set objCurve1 = Nothing
    Set objCurve2 = Nothing
    Set objCurve3 = Nothing
End Sub
See Also

Curve2d Object  | Curve2d Members