Private Sub Form_Load()
Dim objApp As solidedgeframework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objCurves As SolidEdgeFrameworkSupport.Curves2d
Dim objCurve As SolidEdgeFrameworkSupport.Curve2d
Dim dblpoint(1 To 8) As Double
Dim boolCurveClosed As Boolean
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Create Curves2d collection
Set objCurves = objSheet.Curves2d
'Define points
dblpoint(1) = 0.15
dblpoint(2) = 0.15
dblpoint(3) = 0.25
dblpoint(4) = 0.15
dblpoint(5) = 0.25
dblpoint(6) = 0.25
dblpoint(7) = 0.15
dblpoint(8) = 0.25
'Create a curve on the defined points
Set objCurve = objCurves.AddByPoints(Pointcount:=4, Points:=dblpoint, FitType:=igLinestringFit, Closed:=True)
'get Closed value
boolCurveClosed = objCurve.Closed
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objCurves = Nothing
Set objCurve = Nothing
End Sub