Solid Edge FrameworkSupport Type Library
Duplicate Method
Description
Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original.
Syntax
Visual Basic
Public Function Duplicate( _
   Optional ByVal XDistance As Variant, _
   Optional ByVal YDistance As Variant _
) As Object
Parameters
XDistance
YDistance
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCurves As solidedgeframeworksupport.Curves2d
    Dim objCurve1 As solidedgeframeworksupport.Curve2d
    Dim objCurve2 As solidedgeframeworksupport.Curve2d
    Dim dblPoint(1 To 8) As Double
    Dim lngCount1 As Long, lngCount2 As Long, lngCount3 As Long
    Dim lngCount4 As Long, lngCount5 As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create Curves collection
    Set objCurves = objSheet.Curves2d
    'Define points
    dblPoint(1) = 0.15
    dblPoint(2) = 0.15
    dblPoint(3) = 0.25
    dblPoint(4) = 0.15
    dblPoint(5) = 0.25
    dblPoint(6) = 0.25
    dblPoint(7) = 0.15
    dblPoint(8) = 0.25
    'Create curve
    Set objCurve1 = objCurves.AddByPoints(Pointcount:=4, Points:=dblPoint, FitType:=igDirectFit, Closed:=False)
    'Get Count
    lngCount1 = objCurves.Count
    'Duplicate curve
    Set objCurve2 = objCurve1.Duplicate(xdistance:=0.1, ydistance:=0)




    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCurves = Nothing
    Set objCurve1 = Nothing
    Set objCurve2 = Nothing
End Sub
See Also

Curve2d Object  | Curve2d Members