Solid Edge FrameworkSupport Type Library
FitTolerance Property
Description
Sets and returns the fit tolerance of the referenced Curve2d object.
Property type
Read-write property
Syntax
Visual Basic
Public Property FitTolerance As Double
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objCurves As solidedgeframeworksupport.Curves2d
    Dim objCurve1 As solidedgeframeworksupport.Curve2d
    Dim dblPoint(1 To 10) As Double
    Dim dblFitTolerance As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create Curves collection
    Set objCurves = objSheet.Curves2d
    'Define points
    dblPoint(1) = 0.15
    dblPoint(2) = 0.15
    dblPoint(3) = 0.25
    dblPoint(4) = 0.15
    dblPoint(5) = 0.25
    dblPoint(6) = 0.25
    dblPoint(7) = 0.15
    dblPoint(8) = 0.25
    dblPoint(9) = 0.1
    dblPoint(10) = 0.3
    'Create curve
    Set objCurve1 = objCurves.AddByPoints(Pointcount:=5, Points:=dblPoint, FitType:=igLeastSquareFit, Closed:=False)
    'assign FitTolerance
    objCurve1.FitTolerance = 0.0005
    'Get fittolerance
    dblFitTolerance = objCurve1.FitTolerance

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objCurves = Nothing
    Set objCurve1 = Nothing
End Sub
See Also

Curve2d Object  | Curve2d Members