Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objcurves As SolidEdgeFrameworkSupport.Curves2d
    Dim objCurve1 As SolidEdgeFrameworkSupport.Curve2d
    Dim objCurve2 As SolidEdgeFrameworkSupport.Curve2d
    Dim dblPoint(1 To 10) As Double
    Dim lngCurve1Zorder As Long
    Dim lngCurve2Zorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create curves collection
    Set objcurves = objSheet.Curves2d
    'Define points
    dblPoint(1) = 0.15
    dblPoint(2) = 0.15
    dblPoint(3) = 0.25
    dblPoint(4) = 0.15
    dblPoint(5) = 0.25
    dblPoint(6) = 0.25
    dblPoint(7) = 0.15
    dblPoint(8) = 0.25
    dblPoint(9) = 0.1
    dblPoint(10) = 0.1
    'Create curves on the defined points
    Set objCurve1 = objcurves.AddByPoints(Pointcount:=3, Points:=dblPoint, FitType:=igDirectFit, Closed:=True)
    Set objCurve2 = objcurves.AddByPoints(Pointcount:=4, Points:=dblPoint, FitType:=igDirectFit, Closed:=True)
    lngCurve1Zorder = objCurve2.ZOrder
    'Call sendbackward method.
    Call objCurve2.SendBackward



    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objcurves = Nothing
    Set objCurve1 = Nothing
    Set objCurve2 = Nothing
End Sub
See Also

Curve2d Object  | Curve2d Members