Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objCurves As SolidEdgeFrameworkSupport.Curves2d
Dim dblPoint(1 To 8) As Double
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' getting the Curves2d object on the active sheet
Set objCurves = objDoc.ActiveSheet.Curves2d
' Create a Points array to specfy the coordinates of the points as (x1,y1,x2,y2,.......)
dblPoint(1) = 0.1
dblPoint(2) = 0.1
dblPoint(3) = 0.2
dblPoint(4) = 0.1
dblPoint(5) = 0.2
dblPoint(6) = 0.2
dblPoint(7) = 0.1
dblPoint(8) = 0.2
' Creating a Curve2d object by using the above defined points
Call objCurves.AddByPoints(PointCount:=4, Points:=dblPoint)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objCurves = Nothing
End Sub