Solid Edge FrameworkSupport Type Library
Item Method
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As Curve2d
Parameters
Index
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objCurves As SolidEdgeFrameworkSupport.Curves2d
    Dim objCurve2d As SolidEdgeFrameworkSupport.Curve2d
    Dim objCItem As SolidEdgeFrameworkSupport.Curve2d
    Dim dblPoint(1 To 8) As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the Curves2d object on the active sheet
    Set objCurves = objDoc.ActiveSheet.Curves2d
    ' Create a Points array to specfy the coordinates of the points as (x1,y1,x2,y2,.......)
    dblPoint(1) = 0.1
    dblPoint(2) = 0.1
    dblPoint(3) = 0.2
    dblPoint(4) = 0.1
    dblPoint(5) = 0.2
    dblPoint(6) = 0.2
    dblPoint(7) = 0.1
    dblPoint(8) = 0.2
    ' Creating a Curve2d object using the above points
    Set objCurve2d = objCurves.AddByPoints(PointCount:=4, Points:=dblPoint)
    ' getting the particular Curve2d object from the collection object
    Set objCItem = objCurves.Item(Index:=1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objCurves = Nothing
    Set objCurve2d = Nothing
    Set objCItem = Nothing
End Sub
See Also

Curves2d Collection  | Curves2d Members