Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames
Dim objDtmFrm1 As SolidEdgeFrameworkSupport.DatumFrame
Dim objDtmFrm2 As SolidEdgeFrameworkSupport.DatumFrame
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
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' Create a DatumFrames collection object
Set objDatums = objSheet.DatumFrames
' Add a DatumFrame object
Set objDtmFrm1 = objDatums.Add(x1:=0.1, y1:=0.1, z1:=0)
' Assign the Text to the DatumFrame
objDtmFrm1.Datum = "Test"
' Assign the DatumFrame object created to another object
Set objDtmFrm2 = objDatums.Item(Index:=1)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatums = Nothing
Set objDtmFrm1 = Nothing
Set objDtmFrm2 = Nothing
End Sub