Solid Edge FrameworkSupport Type Library
Duplicate Method
Specifies the distance in the x direction from the original that the copy of the referenced object is to be placed.
Specifies the distance in the y direction from the original that the copy of the referenced object is to be placed.
Description
Copies the referenced object to a specified location, creating a new instance of the object with the same property values as the original.
Syntax
Visual Basic
Public Function Duplicate( _
   Optional ByVal XDistance As Variant, _
   Optional ByVal YDistance As Variant _
) As Object
Parameters
XDistance
Specifies the distance in the x direction from the original that the copy of the referenced object is to be placed.
YDistance
Specifies the distance in the y direction from the original that the copy of the referenced object is to be placed.
Remarks
The referenced object is copied to the new location relative to the original (source) location. The distance is the difference from the object's original location to the XDistance and YDistance values. The new object is returned.
See Also

DatumFrame Object  | DatumFrame Members