Solid Edge FrameworkSupport Type Library
Key Property
Description
Returns a key (a string) to find the object relative to its owning parents.
Property type
Read-only property
Syntax
Visual Basic
Public Property Key( _
   Optional ByVal Recurse As Variant _
) As String
Parameters
Recurse
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames
    Dim objDtmFrm As SolidEdgeFrameworkSupport.DatumFrame
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim strKey As String
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Create a Line object
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
    ' Create a DatumFrames collection object
    Set objDatums = objSheet.DatumFrames
    ' Add a DatumFrame object
    Set objDtmFrm = objDatums.AddByTerminator(TerminatorObject:=objLine, _
                                              x1:=0.15, y1:=0.1, z1:=0, keyPoint1:=False)
    objDtmFrm.Datum = "Test"
    ' Get the Key property
    strKey = objDtmFrm.Key
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatums = Nothing
    Set objDtmFrm = Nothing
    Set objLine = Nothing
End Sub
See Also

DatumFrame Object  | DatumFrame Members