Solid Edge FrameworkSupport Type Library
Leader Property
Description
Specifies whether or not the referenced object has a leader line.
Property type
Read-write property
Syntax
Visual Basic
Public Property Leader As Boolean
Remarks
If this property is True, the dimensioning/annotation object has a leader line. For Dimension objects, this property is read-only. For all other objects, this property is read-write. The leader line is valid only when the break is positioned to the left or right of the dimensioning object.
See Also

DatumFrame Object  | DatumFrame Members