Solid Edge FrameworkSupport Type Library
Select Method
Description
Selects the referenced object in the active window.
Syntax
Visual Basic
Public Sub Select() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames
    Dim objDtmFrm As SolidEdgeFrameworkSupport.DatumFrame
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Create a Line object
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
    ' Create a DatumFrames collection object
    Set objDatums = objSheet.DatumFrames
    ' Add a DatumFrame object
    Set objDtmFrm = objDatums.AddByTerminator(TerminatorObject:=objLine, _
                                              x1:=0.15, y1:=0.1, z1:=0, keyPoint1:=False)
    objDtmFrm.Datum = "Test"
    ' Select the DatumFrame
    Call objDtmFrm.Select
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatums = Nothing
    Set objDtmFrm = Nothing
    Set objLine = Nothing
End Sub
See Also

DatumFrame Object  | DatumFrame Members