Solid Edge FrameworkSupport Type Library
SetFreeSpacePoint Method
Specifies the coordinates of the free space point.
Specifies the coordinates of the free space point.
Specifies the coordinates of the free space point.
Description
Specifies the coordinates of the terminal connect point for a leader line belonging to the referenced dimensioning object.
Syntax
Visual Basic
Public Sub SetFreeSpacePoint( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double _
) 
Parameters
x
Specifies the coordinates of the free space point.
y
Specifies the coordinates of the free space point.
z
Specifies the coordinates of the free space point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames
    Dim objDtmFrm As SolidEdgeFrameworkSupport.DatumFrame
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim dblX As Double, dblY As Double, dblZ As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    ' Create a Line object
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
    ' Create a DatumFrames collection object
    Set objDatums = objSheet.DatumFrames
    ' Add a DatumFrame object
    Set objDtmFrm = objDatums.AddByTerminator(TerminatorObject:=objLine, _
                                              x1:=0.15, y1:=0.1, z1:=0, keyPoint1:=False)
    objDtmFrm.Datum = "Test"
    ' Add Vertex to the object
    Call objDtmFrm.AddVertex(x:=0.3, y:=0.2, z:=0)
    Call objDtmFrm.AddVertex(x:=0.4, y:=0.1, z:=0)
    ' Set the Free Space Point
    Call objDtmFrm.SetFreeSpacePoint(x:=0.2, y:=0.3, z:=0)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatums = Nothing
    Set objDtmFrm = Nothing
    Set objLine = Nothing
End Sub
See Also

DatumFrame Object  | DatumFrame Members