Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatums As SolidEdgeFrameworkSupport.DatumFrames
Dim objDtmFrm As SolidEdgeFrameworkSupport.DatumFrame
Dim objLine As SolidEdgeFrameworkSupport.Line2d
Dim objCircle As SolidEdgeFrameworkSupport.Circle2d
Dim objTermObject As Object
Dim dblX As Double, dblY As Double, dblZ As Double
Dim bKeyPt As Boolean
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
' Create a Line object
Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
' Create a DatumFrames collection object
Set objDatums = objSheet.DatumFrames
' Add a DatumFrame object
Set objDtmFrm = objDatums.AddByTerminator(TerminatorObject:=objLine, _
x1:=0.15, y1:=0.1, z1:=0, keyPoint1:=False)
objDtmFrm.Datum = "Test"
' Create a Circle
Set objCircle = objSheet.Circles2d.AddByCenterRadius(x:=0.2, y:=0.3, Radius:=0.06)
' Set the Terminator object
Call objDtmFrm.SetTerminator(TerminatorObj:=objCircle, _
x:=0.26, y:=0.3, z:=0, Keypoint:=False)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatums = Nothing
Set objDtmFrm = Nothing
Set objLine = Nothing
Set objCircle = Nothing
End Sub