Solid Edge FrameworkSupport Type Library
Item Method
Variant (input) index.
Description
The items in a collection.
Syntax
Visual Basic
Public Function Item( _
   ByVal Index As Variant _
) As DatumPoint
Parameters
Index
Variant (input) index.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objDatumPoint1 As SolidEdgeFrameworkSupport.DatumPoint
    Dim objDatumPoint2 As SolidEdgeFrameworkSupport.DatumPoint
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a datumpoints collection
    Set objDatumPoints = objSheet.DatumPoints
    'add a datumpoint to collection
    Set objDatumPoint1 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'get the object thru item method
    Set objDatumPoint2 = objDatumPoints.Item(Index:=1)



    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objDatumPoint1 = Nothing
    Set objDatumPoint2 = Nothing
End Sub
See Also

DatumPoints Collection  | DatumPoints Members