Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-write property
Syntax
Visual Basic
Public Property Style As DimensionStyle
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objMyDimStyle As Object
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'add a new style
    Set objMyDimStyle = objDoc.DimensionStyles.Add("MyStyle", "ISO")
    'create the datumpoints collection
    Set objDatumPoints = objSheet.DatumPoints
    'set style
    objDatumPoints.Style = objMyDimStyle
    'get the style
    Set objStyle = objDatumPoints.Style




    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objStyle = Nothing
End Sub
See Also

DatumPoints Collection  | DatumPoints Members