Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objDatumPoint As SolidEdgeFrameworkSupport.DatumPoint
    Dim objDatumPtApp As SolidEdgeFramework.Application
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create datumpoints collection.
    Set objDatumPoints = objSheet.DatumPoints
    'create a datumpoint
    Set objDatumPoint = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'get application
    Set objDatumPtApp = objDatumPoint.Application




    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objDatumPoint = Nothing
    Set objDatumPtApp = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members