Solid Edge FrameworkSupport Type Library
BringForward Method
Description
Changes the display order of the referenced object by moving it in front of the first object that obscures it.
Syntax
Visual Basic
Public Sub BringForward() 
Remarks
This command is useful when other objects that are filled hide an object and the user wants to remove the object from hiding while not bringing the object to the top of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objdatumpoint1 As SolidEdgeFrameworkSupport.DatumPoint
    Dim objdatumpoint2 As SolidEdgeFrameworkSupport.DatumPoint
    Dim lngZorder1 As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a collection of datumpoints
    Set objDatumPoints = objSheet.DatumPoints
    'add a datumpoint to collection
    Set objdatumpoint1 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'add one more datumpoint to collection
    Set objdatumpoint2 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'get zorder
    lngZorder1 = objdatumpoint1.ZOrder
    'Bringforward datumpoint1
    Call objdatumpoint1.BringForward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objdatumpoint1 = Nothing
    Set objdatumpoint2 = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members