Solid Edge FrameworkSupport Type Library
BringToFront Method
Description
Changes the display order of the referenced object by moving it in front of all other overlapping objects.
Syntax
Visual Basic
Public Sub BringToFront() 
Remarks
This command is useful when objects are hidden by other objects that are filled and have a higher priority display. The BringForward method can also be used.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objdatumpoint1 As SolidEdgeFrameworkSupport.DatumPoint
    Dim objdatumpoint2 As SolidEdgeFrameworkSupport.DatumPoint
    Dim objdatumpoint3 As SolidEdgeFrameworkSupport.DatumPoint
    Dim lngZorder1 As Long
    Dim lngZorder2 As Long
    Dim lngZorder3 As Long
    Dim lngZorder4 As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a collection of datumpoints
    Set objDatumPoints = objSheet.DatumPoints
    'add datumpoints
    Set objdatumpoint1 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    Set objdatumpoint2 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    Set objdatumpoint3 = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'get zorder of first datumpoint
    lngZorder1 = objdatumpoint1.ZOrder
    'bring to front
    Call objdatumpoint1.BringToFront
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objdatumpoint1 = Nothing
    Set objdatumpoint2 = Nothing
    Set objdatumpoint3 = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members