Solid Edge FrameworkSupport Type Library
Name Property
Description
Returns the name of the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Name( _
   Optional ByVal Recurse As Variant _
) As String
Parameters
Recurse
Remarks
All objects have names that are unique within the scope of their parent.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
    Dim objdatumPoint As SolidEdgeFrameworkSupport.DatumPoint
    Dim strName As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'create a collection of datumpoints
    Set objDatumPoints = objSheet.DatumPoints
    'add a datumpoint to collection
    Set objdatumPoint = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
    'get name
    strName = objdatumPoint.Name
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumPoints = Nothing
    Set objdatumPoint = Nothing
End Sub
See Also

DatumPoint Object  | DatumPoint Members