Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints
Dim objDatumPoint As SolidEdgeFrameworkSupport.DatumPoint
Dim lngPointType As SolidEdgeConstants.DimDatumPointTypeConstants
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Get the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'create a datumpoints' collection.
Set objDatumPoints = objSheet.DatumPoints
'add a datumpoint to collection
Set objDatumPoint = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0)
'get pointType
lngPointType = objDatumPoint.PointType
'Change the PointType to Circle
objDatumPoint.PointType = igDimDatumPointCircle
'Set the AreaSize to soem value so that DatumPoint can be seen
objDatumPoint.AreaSize = 0.01
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatumPoints = Nothing
Set objDatumPoint = Nothing
End Sub