| Solid Edge FrameworkSupport Type Library > DatumPoint Object : Style Property |
| Visual Basic |
|---|
Public Property Style As DimStyle |
Private Sub Form_Load() Dim objApp As SolidEdgeFrameWork.Application Dim objDoc As SolidEdgeDraft.DraftDocument Dim objSheet As SolidEdgeDraft.Sheet Dim objDatumPoints As SolidEdgeFrameworkSupport.DatumPoints Dim objDatumPoint As SolidEdgeFrameworkSupport.DatumPoint Dim objStyle As SolidEdgeFrameworkSupport.DimStyle ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If 'Get the Active Sheet object Set objSheet = objDoc.ActiveSheet 'create datumpoints collection Set objDatumPoints = objSheet.DatumPoints 'add a datumpoint to collection Set objDatumPoint = objDatumPoints.Add(x1:=0.2, y1:=0.2, z1:=0) 'get style Set objStyle = objDatumPoint.Style ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objSheet = Nothing Set objDatumPoints = Nothing Set objDatumPoint = Nothing Set objStyle = Nothing End Sub