Solid Edge FrameworkSupport Type Library
AddByTerminator Method
Specifies the object to which the terminal end of the leader connects.
Specifies the coordinates of the leader's start locate point. This point is used as a proximity point while calculating the key point. The z1 argument applies only to 3-D objects.
Specifies the coordinates of the leader's start locate point. This point is used as a proximity point while calculating the key point. The z1 argument applies only to 3-D objects.
Specifies the coordinates of the leader's start locate point. This point is used as a proximity point while calculating the key point. The z1 argument applies only to 3-D objects.
Specifies whether the object or a key point of the TerminatorObject is to be considered. If KeyPoint1 is True, the leader's terminal end is placed with respect to the TerminatorObject; if KeyPoint1 is False, the nearest key point on that object is selected.
Description
Creates a Leader or annotation object with a Leader.
Syntax
Visual Basic
Public Function AddByTerminator( _
   ByVal TerminatorObject As Object, _
   ByVal x1 As Double, _
   ByVal y1 As Double, _
   ByVal z1 As Double, _
   ByVal keyPoint1 As Boolean _
) As DatumTarget
Parameters
TerminatorObject
Specifies the object to which the terminal end of the leader connects.
x1
Specifies the coordinates of the leader's start locate point. This point is used as a proximity point while calculating the key point. The z1 argument applies only to 3-D objects.
y1
Specifies the coordinates of the leader's start locate point. This point is used as a proximity point while calculating the key point. The z1 argument applies only to 3-D objects.
z1
Specifies the coordinates of the leader's start locate point. This point is used as a proximity point while calculating the key point. The z1 argument applies only to 3-D objects.
keyPoint1
Specifies whether the object or a key point of the TerminatorObject is to be considered. If KeyPoint1 is True, the leader's terminal end is placed with respect to the TerminatorObject; if KeyPoint1 is False, the nearest key point on that object is selected.
Remarks
To create the annotation object with this method, specify the object to which the leader connects. As a result of this method, the annotation object is automatically positioned with respect to the object to which the leader connects.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
    Dim objDatumTarget1 As SolidEdgeFrameworkSupport.DatumTarget
    Dim lngCountbfr As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create a Line2d
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.25, y1:=0.25, x2:=0.45, y2:=0.25)
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    lngCountbfr = objDatumTargets.Count
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.AddByTerminator(TerminatorObject:=objLine, _
                                                         x1:=0.3, y1:=0.25, z1:=0, keypoint1:=False)
    'Add a Text to the Datum Target
    objDatumTarget.DatumReference = "A"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
    Set objDatumTarget1 = Nothing
    Set objLine = Nothing
End Sub
See Also

DatumTargets Collection  | DatumTargets Members