Solid Edge FrameworkSupport Type Library
ClearStyle Method
Description
Clears any previously set style object.
Syntax
Visual Basic
Public Sub ClearStyle() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objANSIStyle As SolidEdgeFrameworkSupport.DimensionStyle
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a dimension style
    Set objANSIStyle = objDoc.DimensionStyles.Add(Name:="MyDimStyle", Parent:="ANSI")
    'Set the STyle to ANSI
    objDatumTargets.Style = objANSIStyle
    'Clear the Objectstyle
    Call objDatumTargets.ClearStyle
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objANSIStyle = Nothing
End Sub
See Also

DatumTargets Collection  | DatumTargets Members