Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
    Dim objApplication As SolidEdgeFrameWork.Application
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Add a Text to the Datum Target
    objDatumTarget.DatumReference = "A"
    'Get the Application
    Set objApplication = objDatumTarget.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
    Set objApplication = Nothing
End Sub
See Also

DatumTarget Object  | DatumTarget Members