Solid Edge FrameworkSupport Type Library
Copy Method
Description
Places a copy of the referenced object on the clipboard.
Syntax
Visual Basic
Public Sub Copy() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Add a Text to the Datum Target
    objDatumTarget.DatumReference = "A"
    'Copy the DatumTarget object to the clipboard
    Call objDatumTarget.Copy
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
End Sub
See Also

DatumTarget Object  | DatumTarget Members