Private Sub Form_Load()
Dim objApp As SolidEdgeFrameWork.Application
Dim objDoc As SolidEdgeDraft.DraftDocument
Dim objSheet As SolidEdgeDraft.Sheet
Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
Dim cLeaderType As SolidEdgeConstants.DimDatumTargetLeaderTypeConstants
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'getting the Active Sheet object
Set objSheet = objDoc.ActiveSheet
'Getting the DatumTargets object
Set objDatumTargets = objSheet.DatumTargets
'Create a Datum target in the active sheet
Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
'Set the DatumReference
objDatumTarget.DatumReference = "A"
'Add a vertex
Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
'Get the Leader Type
cLeaderType = objDatumTarget.LeaderType
'Set the leader type to Far side
objDatumTarget.LeaderType = igDimDatumTargetFarSide
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objSheet = Nothing
Set objDatumTargets = Nothing
Set objDatumTarget = Nothing
End Sub