Solid Edge FrameworkSupport Type Library
SetTerminator Method
Specifies the annotation object to which the leader is to be connected.
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
Specifies whether the object or a key point of the terminator object is to be used. If True, the leader's terminal end is placed with respect to the TerminatorObject; if False, the nearest key point on that object is selected.
Description
Specifies a new object and/or connect point for the terminal end of an annotatino object's leader.
Syntax
Visual Basic
Public Sub SetTerminator( _
   ByVal TerminatorObj As Object, _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double, _
   ByVal keyPoint As Boolean _
) 
Parameters
TerminatorObj
Specifies the annotation object to which the leader is to be connected.
x
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
y
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
z
Coordinates of the locate point for the terminator object. This point is used as a proximity point while calculating the key point.
keyPoint
Specifies whether the object or a key point of the terminator object is to be used. If True, the leader's terminal end is placed with respect to the TerminatorObject; if False, the nearest key point on that object is selected.
Remarks
If the annotation object is placed with respect to a key point, the point of reference is the key point.
See Also

DatumTarget Object  | DatumTarget Members