Solid Edge FrameworkSupport Type Library
SetVertex Method
The index, relative to zero, of the vertex number in the object. This value must be between one and the number of vertices.
Specifies the new coordinates for the vertex.
Specifies the new coordinates for the vertex.
Specifies the new coordinates for the vertex.
Description
Sets the coordinates of an existing vertex of the referenced object.
Syntax
Visual Basic
Public Sub SetVertex( _
   ByVal Index As Long, _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal z As Double _
) 
Parameters
Index
The index, relative to zero, of the vertex number in the object. This value must be between one and the number of vertices.
x
Specifies the new coordinates for the vertex.
y
Specifies the new coordinates for the vertex.
z
Specifies the new coordinates for the vertex.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objDatumTargets As SolidEdgeFrameworkSupport.DatumTargets
    Dim objDatumTarget As SolidEdgeFrameworkSupport.DatumTarget
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Getting the DatumTargets object
    Set objDatumTargets = objSheet.DatumTargets
    'Create a Datum target in the active sheet
    Set objDatumTarget = objDatumTargets.Add(x1:=0.3, y1:=0.25, z1:=0.25)
    'Set the DatumReference property
    objDatumTarget.DatumReference = "A"
    'Add a vertex at the end
    Call objDatumTarget.AddVertex(x:=0.35, y:=0.3, z:=0)
    Call objDatumTarget.AddVertex(x:=0.45, y:=0.2, z:=0)
    'Set the vertex of Datumtarget
    Call objDatumTarget.SetVertex(Index:=1, x:=0.4, y:=0.25, z:=0)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objDatumTargets = Nothing
    Set objDatumTarget = Nothing
End Sub
See Also

DatumTarget Object  | DatumTarget Members