| Solid Edge FrameworkSupport Type Library : DimInitData Object |
ClearAxis | Clears the dimension axis. |
ClearCreationData | Resets all the data in this DimInitData object. |
ClearParents | Clears the parent data and sets the number of parents to zero. Use between calls to CreateDimension. |
ClearPlane | Clears the dimension plane. |
SetAngularCoordinateCounterClockwise | Set TRUE to create an angular dimension that reads counterclockwise. This is specific to angular coordinate dimensions. |
SetAngularCoordOrigin | Set TRUE if creating an angular coordinate origin dimension. |
SetAxis | Sets the dimension axis and will be used by explicit axis dimensions. The axis mode can be set by using the method SetAxisMode. |
SetAxisMode | Sets the axis mode. Not used when creating a Chamfer Dimension, use SetChamferAxisMode instead. |
SetChamferAxisMode | Sets the chamfer axis mode. Use when creating a Chamfer Dimension. |
SetDimPosition | Sets the position of the dimension. This works in conjunction with SetDimPositionMode. |
SetDimPositionMode | Set TRUE to specify whether to use SetDimPosition value to position the coordinate and angular coordinate dimensions when created. Set FALSE to use default position. |
SetNumberOfParents | Sets the number of parents with which the dimension will be created. |
SetParentByIndex | Sets parent data. Object must be 2d geometry, reference, or edge or vertex (for PMI). For coordinate dimensions (except the origin), the first parent must be a dimension object that belongs to the group. UseVirtualVertex is used for PMI. |
SetPlane | Sets the plane in which the dimension will be created. This is used only for creating PMI dimensions. (XY plane is the default plane) |
SetTrue3DSketchDimension | Set TRUE to create a True dimension for a 3D sketch line or between 2 elements (one of which is a 3D sketch element). This is specific to 3D sketch dimensions. |
SetType | Sets the type of dimension. |
Application | Returns the active application object. |