Solid Edge FrameworkSupport Type Library
Add Method
Specifies the name for the new style.
Specifies the name of an existing style on which the new style is to be based.
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal Name As String, _
   ByVal Parent As String _
) As DimensionStyle
Parameters
Name
Specifies the name for the new style.
Parent
Specifies the name of an existing style on which the new style is to be based.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objDimStyles As SolidEdgeFrameworkSupport.DimensionStyles
    Dim objANSImmDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objANSIDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objISODimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objBSIDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objDINDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objJISDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
    Dim objUNIDimStyle As SolidEdgeFrameworkSupport.DimensionStyle
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the DimensionsStyles collection object
    Set objDimStyles = objDoc.DimensionStyles
    'Add a New DimStyle
    Set objANSImmDimStyle = objDimStyles.Add(Name:="DimStyle1", Parent:="ANSImm")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objDimStyles = Nothing
    Set objANSImmDimStyle = Nothing
    Set objANSIDimStyle = Nothing
    Set objISODimStyle = Nothing
    Set objBSIDimStyle = Nothing
    Set objDINDimStyle = Nothing
    Set objJISDimStyle = Nothing
    Set objUNIDimStyle = Nothing
End Sub
See Also

DimensionStyles Collection  | DimensionStyles Members