Solid Edge FrameworkSupport Type Library
AngularUnits Property
Description
Sets and returns the angular dimensioning unit separate from the working units of the file.
Property type
Read-write property
Syntax
Visual Basic
Public Property AngularUnits As DimAngularUnitConstants
Remarks
Valid values are members of the DimAngularUnitConstants constant set.
See Also

DimensionStyle Object  | DimensionStyle Members