Sets and returns the color in which driving dimensions are displayed.
Property type
Read-write property
Syntax
Visual Basic
Public Property DrivingColor As Long
Remarks
When an equation constraint is assigned to make a driving dimension a function of another dimension, a variable, or an equation, the color of the text of the driving dimension will assume the driven dimension color. If the relationship is removed, the text again assumes the driving dimension color.