Solid Edge FrameworkSupport Type Library
LeaderLineLength Property
Description
Sets and returns the default leader distance.
Property type
Read-write property
Syntax
Visual Basic
Public Property LeaderLineLength As Double
Remarks
The value is a ratio of dimension text height. The leader line is valid only when the break is positioned to the left or right of the associated Dimension object.
See Also

DimensionStyle Object  | DimensionStyle Members