Solid Edge FrameworkSupport Type Library
OffsetLeaderType Property
Description
Sets and returns the type of offset leader to be drawn.
Property type
Read-write property
Syntax
Visual Basic
Public Property OffsetLeaderType As DimOffsetLeaderTypeConstants
Remarks
The Offset Leader Line is valid only when the text is offset.
See Also

DimensionStyle Object  | DimensionStyle Members