Solid Edge FrameworkSupport Type Library
ProjectionExtensionGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimensionStyle Object
: ProjectionExtensionGap Property
Description
Sets and returns the distance by which the projection lines are extended beyond the dimension line.
Property type
Read-write property
Syntax
Visual Basic
Public Property ProjectionExtensionGap As Double
Remarks
The extension gap value is a ratio of dimension text height.
See Also
DimensionStyle Object
|
DimensionStyle Members