Solid Edge FrameworkSupport Type Library
TextClearanceGap Property
Description
Sets and returns the gap distance between the dimension text and the dimension line.
Property type
Read-write property
Syntax
Visual Basic
Public Property TextClearanceGap As Double
Remarks
The text clearance gap value is a ratio of dimension text height.
See Also

DimensionStyle Object  | DimensionStyle Members