Solid Edge FrameworkSupport Type Library
Circumference Property
Description
Returns the dimension along the line of a circle or ellipse.
Property type
Read-only property
Syntax
Visual Basic
Public Property Circumference As Double
Remarks
The circumference value is always around the complete object for objects that are partially trimmed or hidden.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim dblCircum As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0.04, yCenter:=0.03, xMajor:= _
                                             0.01, yMajor:=0.01, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' Get the Circumference Property
    dblCircum = objEllipse.Circumference
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members