Solid Edge FrameworkSupport Type Library
Key Property
Description
Returns a key (a string) to find the object relative to its owning parents.
Property type
Read-only property
Syntax
Visual Basic
Public Property Key( _
   Optional ByVal Recurse As Variant _
) As String
Parameters
Recurse
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim strKey As String
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0.04, yCenter:=0.03, xMajor:= _
                                             0.01, yMajor:=0.01, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' Get the Key Property of the Ellipse
    strKey = objEllipse.Key
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members