Solid Edge FrameworkSupport Type Library
Mirror Method
Specifies the x coordinate of the first point on the mirror axis.
Specifies the y coordinate of the first point on the mirror axis.
Specifies the x coordinate of the second point on the mirror axis.
Specifies the y coordinate of the second point on the mirror axis.
Specifies whether or not the copied object will be active.
Description
Copies the referenced object about an axis.
Syntax
Visual Basic
Public Function Mirror( _
   ByVal x1 As Double, _
   ByVal y1 As Double, _
   ByVal x2 As Double, _
   ByVal y2 As Double, _
   Optional ByVal BooleanCopyFlag As Variant _
) As Object
Parameters
x1
Specifies the x coordinate of the first point on the mirror axis.
y1
Specifies the y coordinate of the first point on the mirror axis.
x2
Specifies the x coordinate of the second point on the mirror axis.
y2
Specifies the y coordinate of the second point on the mirror axis.
BooleanCopyFlag
Specifies whether or not the copied object will be active.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0.04, yCenter:=0.03, xMajor:= _
                                             0.01, yMajor:=0.01, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' Make a Mirror of the Ellipse object
    Call objEllipse.Mirror(x1:=0, y1:=0, x2:=0.1, y2:=0)
    If objEllipses.Count <> 1 Then
        MsgBox ("Mirror method of Ellipse2d object failed")
    End If
    ' Make a Mirror of the Ellipse object
    Call objEllipse.Mirror(x1:=0, y1:=0, x2:=0.1, y2:=0, BooleanCopyFlag:=True)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members