Solid Edge FrameworkSupport Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim objParent As SolidEdgePart.Profile
    Dim objProf As SolidEdgePart.Profile
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProf = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                      objDoc.RefPlanes(1))
    'Create an Ellipses collection object
    Set objEllipses = objProf.Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0.04, yCenter:=0.03, xMajor:= _
                                             0.01, yMajor:=0.01, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' Get the Parent Property
    Set objParent = objEllipse.Parent
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
    Set objParent = Nothing
    Set objProf = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members