Solid Edge FrameworkSupport Type Library
RemoveAllSegmentedStyles Method
Description
Removes all segments defined for the referenced graphic object.
Syntax
Visual Basic
Public Sub RemoveAllSegmentedStyles() 
Remarks
Removing segmented styles does not remove the geometry. Instead, it removes the linear styles applied to the graphic object defined by the segments. If a segment is blank (for example, when the linear style is null), it reappears when its segment is removed.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objEllipses2d As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse2d As SolidEdgeFrameworkSupport.Ellipse2d
    Dim objLinearStyles As SolidEdgeFrameWork.LinearStyles
    Dim objLinearStyle As SolidEdgeFrameWork.LinearStyle
    Dim objLinearStyle1 As SolidEdgeFrameWork.LinearStyle
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'getting the Ellipses2d object
    Set objEllipses2d = objSheet.Ellipses2d
    'Create an Ellispse2d in Clockwise orientation
    Set objEllipse2d = objEllipses2d.AddByCenter(xCenter:=0.3, yCenter:=0.25, _
                                                 xMajor:=0.1, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    'Get the LinearStyles object
    Set objLinearStyles = objDoc.LinearStyles
    'Add new LinearStyles to the collection
    Set objLinearStyle = objLinearStyles.Add(Name:="LinearStyle1", Parent:="Visible")
    Set objLinearStyle1 = objLinearStyles.Add(Name:="LinearStyle2", Parent:="Tangent")
    'set the color property to blue
    objLinearStyle.Color = vbBlue
    'create segements with LinearStyles
    Call objEllipse2d.AddSegmentedStyle(x1:=0.25, y1:=0.25, x2:=0.3, y2:=0.3, Style:=objLinearStyle)
    Call objEllipse2d.AddSegmentedStyle(x1:=0.35, y1:=0.25, x2:=0.3, y2:=0.2, Style:=objLinearStyle1)
    'Remove all segmented styles
    Call objEllipse2d.RemoveAllSegmentedStyles
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objEllipses2d = Nothing
    Set objEllipse2d = Nothing
    Set objLinearStyles = Nothing
    Set objLinearStyle1 = Nothing
    Set objLinearStyle = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members