Solid Edge FrameworkSupport Type Library
Rotate Method
Specifies, in radians, the angle of rotation.
Specifies the x coordinate for the point of rotation.
Specifies the y coordinate for the point of rotation.
Description
Rotates the referenced object about the point specified by the angle in radians.
Syntax
Visual Basic
Public Sub Rotate( _
   ByVal Angle As Double, _
   ByVal x As Double, _
   ByVal y As Double _
) 
Parameters
Angle
Specifies, in radians, the angle of rotation.
x
Specifies the x coordinate for the point of rotation.
y
Specifies the y coordinate for the point of rotation.
Remarks
If the object is to be rotated about its center point, the origin must be set to its center point.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim x As Double, y As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0.1, yCenter:=0, xMajor:= _
                                             0.01, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' Rotate the Ellipse by 90 degrees
    Call objEllipse.Rotate(Angle:=PI / 2, x:=0, y:=0)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members