Solid Edge FrameworkSupport Type Library
SendBackward Method
Description
Changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Syntax
Visual Basic
Public Sub SendBackward() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display but when you do not want to send the object all the way to the back of the priority list.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse1 As SolidEdgeFrameworkSupport.Ellipse2d
    Dim objEllipse2 As SolidEdgeFrameworkSupport.Ellipse2d
    Dim objEllipse3 As SolidEdgeFrameworkSupport.Ellipse2d
    Dim objEllipse4 As SolidEdgeFrameworkSupport.Ellipse2d
    Dim lngZorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the Ellipses2d object
    Set objEllipses = objSheet.Ellipses2d
    'Create an ellipse2d object
    Set objEllipse1 = objEllipses.AddByCenter(xCenter:=0.3, yCenter:=0.25, _
                                              xMajor:=0.1, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    Set objEllipse2 = objEllipses.AddByCenter(xCenter:=0.3, yCenter:=0.25, _
                                              xMajor:=0.08, yMajor:=0, Ratio:=0.3, Orientation:=igGeom2dOrientClockwise)
    Set objEllipse3 = objEllipses.AddByCenter(xCenter:=0.15, yCenter:=0.15, _
                                              xMajor:=0.1, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    Set objEllipse4 = objEllipses.AddByCenter(xCenter:=0.15, yCenter:=0.15, _
                                              xMajor:=0.08, yMajor:=0, Ratio:=0.3, Orientation:=igGeom2dOrientClockwise)
    lngZorder = objEllipse4.ZOrder
    Call objEllipse4.SendBackward
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objEllipses = Nothing
    Set objEllipse1 = Nothing
    Set objEllipse2 = Nothing
    Set objEllipse3 = Nothing
    Set objEllipse4 = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members