Solid Edge FrameworkSupport Type Library
SetMinorAxis Method
Specifies the x value of the minor axis vector.
Specifies the y value of the minor axis vector.
Description
Sets the x and y values of the minor axis vector for the referenced object.
Syntax
Visual Basic
Public Sub SetMinorAxis( _
   ByVal x As Double, _
   ByVal y As Double _
) 
Parameters
x
Specifies the x value of the minor axis vector.
y
Specifies the y value of the minor axis vector.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse As SolidEdgeFrameworkSupport.Ellipse2d
    Dim x As Double, y As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an Ellipses collection object
    Set objEllipses = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).Ellipses2d
    'Create an Ellipse object
    Set objEllipse = objEllipses.AddByCenter(xCenter:=0, yCenter:=0, xMajor:= _
                                             0.01, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' Set the MinorAxis of the Ellipse
    Call objEllipse.SetMinorAxis(x:=0, y:=0.05)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllipses = Nothing
    Set objEllipse = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members