Solid Edge FrameworkSupport Type Library
ZOrder Property
Description
Specifies the front-to-back order in which an object is displayed relative to other objects.
Property type
Read-only property
Syntax
Visual Basic
Public Property ZOrder As Long
Remarks
This relationship is maintained by storing a cardinal order position on each object. An object with a higher cardinal order is displayed in front of one with a lower cardinal number. A change in an object's ZOrder changes how objects are displayed if filled objects are displayed over other objects. The value assigned to this property can be changed internally to maintain unique values on all objects. Therefore, the value returned for this property may not be the same value to which the property was set.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objEllipses As SolidEdgeFrameworkSupport.Ellipses2d
    Dim objEllipse1 As SolidEdgeFrameworkSupport.Ellipse2d
    Dim objLines As SolidEdgeFrameworkSupport.Lines2d
    Dim objline As SolidEdgeFrameworkSupport.Line2d
    Dim lngZorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the Lines2d object
    Set objLines = objSheet.Lines2d
    'Create a line crsoosing the ellipse
    Set objline = objLines.AddBy2Points(x1:=0.15, y1:=0.25, x2:=0.45, y2:=0.25)
    'Get ZOrder of the Line object
    lngZorder = objline.ZOrder
    'Get the Ellipses2d object
    Set objEllipses = objSheet.Ellipses2d
    'Create an ellipse2d object
    Set objEllipse1 = objEllipses.AddByCenter(xCenter:=0.3, yCenter:=0.25, _
                                              xMajor:=0.1, yMajor:=0, Ratio:=0.5, Orientation:=igGeom2dOrientClockwise)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objEllipses = Nothing
    Set objEllipse1 = Nothing
    Set objLines = Nothing
    Set objline = Nothing
End Sub
See Also

Ellipse2d Object  | Ellipse2d Members