Solid Edge FrameworkSupport Type Library
Extend Method
Double that specifies the coordinates of the point at which the referenced element is to be extended.
Double that specifies the coordinates of the point at which the referenced element is to be extended.
The object to which the referenced element is to extend.
Description
Extends open graphic elements to a specified location.
Syntax
Visual Basic
Public Sub Extend( _
   ByVal x As Double, _
   ByVal y As Double, _
   ByVal TargetObj As Object _
) 
Parameters
x
Double that specifies the coordinates of the point at which the referenced element is to be extended.
y
Double that specifies the coordinates of the point at which the referenced element is to be extended.
TargetObj
The object to which the referenced element is to extend.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 0 * PI / 180
    dblFin = 90 * PI / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0, yCenter:=0, _
                                             xMajoraxis:=0.04, yMajoraxis:=0, Ratio:=0.5, _
                                             Orientation:=1, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Create a Line object
    Set objLine1 = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                       objDoc.RefPlanes(1)).Lines2d.AddBy2Points(x1:=-0.04, _
                                                                                                 y1:=0, x2:=0, y2:=0)
    ' Extend the EllipticalArc to the Line object
    Call objEllpArc.Extend(x:=0, y:=0.02, TargetObj:=objLine1)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
    Set objLine1 = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members