Solid Edge FrameworkSupport Type Library
Parent Property
Description
Returns the parent object for the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Parent As Object
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim objParent As SolidEdgePart.Profile
    Dim objProf As SolidEdgePart.Profile
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile object
    Set objProf = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                      objDoc.RefPlanes(1))
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objProf.EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0.02, yCenter:=0.02, _
                                             xMajoraxis:=0.03, yMajoraxis:=0.02, Ratio:=0.5, _
                                             Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Get the Parent Property
    Set objParent = objEllpArc.Parent
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
    Set objParent = Nothing
    Set objProf = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members