Solid Edge FrameworkSupport Type Library
RotationAngle Property
Description
Sets and returns the angle, in radians, at which the object is rotated along its major axis.
Property type
Read-write property
Syntax
Visual Basic
Public Property RotationAngle As Double
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEllpArcs As SolidEdgeFrameworkSupport.EllipticalArcs2d
    Dim objEllpArc As SolidEdgeFrameworkSupport.EllipticalArc2d
    Dim dblStrt As Double
    Dim dblFin As Double
    Dim dblRotAng As Double
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Create an EllipticalArcs2d collection object
    Set objEllpArcs = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                          objDoc.RefPlanes(1)).EllipticalArcs2d
    'Create an EllipticalArc object
    dblStrt = 180 * PI / 180
    dblFin = 230 * PI / 180
    Set objEllpArc = objEllpArcs.AddByCenter(xCenter:=0, yCenter:=0, _
                                             xMajoraxis:=0.03, yMajoraxis:=0, Ratio:=0.5, _
                                             Orientation:=0, StartAngle:=dblStrt, EndAngle:=dblFin)
    ' Get the RotationAngle of the EllipticalArc object
    dblRotAng = objEllpArc.RotationAngle
    objEllpArc.RotationAngle = PI / 2
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEllpArcs = Nothing
    Set objEllpArc = Nothing
End Sub
See Also

EllipticalArc2d Object  | EllipticalArc2d Members